Viewing Event Logs - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

About this task

You can perform this task only in Commissioning mode.

Procedure

  1. Start the tool and open the controller application.
  2. Click the Advanced tab.
  3. In the Advanced Object tree under Intrinsic Alarming, click Event Log and then click the Events tab. A list of events appear.
    Note:

    Click the columns to sort the list of events.

    To copy details from the event into another program, select the row and click Copy to Clipboard.

    To refresh the screen, click the lightning button on top left of the Events tab.