Referencing a Global Calendar - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

About this task

If necessary, you can reference a calendar on a different device or another calendar on the same device.

Procedure

  1. Start the tool and open the controller application.
  2. Click the Advanced tab.
  3. In the Advanced Object tree, right-click Calendars and click Add Calendar. A new calendar is added to the Advanced Object tree.
  4. Click the calendar located below Calendars in the Advanced Object tree.
  5. Click Edit. The fields you can edit appear in white.
  6. Enter basic information for the calendar.
  7. Next to the Date List field, click Add. The Calendar View window appears.
  8. Select Global.
  9. In the Device field, enter the BACnet global identifier of the device.
  10. In the Calendar field, enter the BACnet global identifier of the calendar.
  11. Click Apply.