Adding a Basic Calendar - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

About this task

Calendars work in conjunction with schedules by allowing you to specify the days when you want an exception schedule to be active. One common use of calendars is to indicate holiday days when an alternative occupancy schedule is in effect.

Procedure

  1. Start the tool and open the controller application.
  2. Click the Advanced tab.
  3. In the Advanced Object tree, right-click Calendars and click Add Calendar. A new calendar is added to the Advanced Object tree.
  4. Click the calendar located below Calendars in the Advanced Object tree.
  5. Click Edit. The fields you can edit appear in white.
  6. Enter basic information for the calendar. See Calendar Details Screen.
  7. Next to the Date List field, click Add. The Calendar View window appears.
  8. Select the days you want to add to the calendar. See Calendar View for more information about the buttons in the calendar.
  9. Click Save.
  10. Click Apply.