The Chart view allows you to view data samples in chart format. You can zoom in, zoom out, and pan within the chart.
Button |
View |
Description |
---|---|---|
|
Update |
Retrieves the most recent data samples for the displayed trends. |
|
Zoom |
Toggles the mouse behavior for the chart between zoom mode and normal mode. While in zoom mode:
When you exit zoom mode, the chart remains at the current zoom level. Use the Restore button to fully zoom out. Notes:
|
|
Restore |
Use to return to a zoomed out view and switches the mouse back to normal mode when the chart's zoom mode is active. |
|
Points Line |
Data using lines and point markers. This is the default behavior. |
|
Area |
Data using an area chart. |
|
Bar |
Data using a bar chart. Note: Use the bar chart only when the number of data samples can reasonably be expected to display as bars. If too many data samples exist when you click this option, the display becomes unstable and fails to properly update the screen. To recover, select any other display option.
|
|
Points |
Data using markers with no lines. |
|
Line |
Data using lines with no markers. |
|
Stacked Y Axis |
Displays each trend on a separate Y axis. This option is not available when viewing a single trend. |
|
Single Y Axis |
Displays each trend with the same Y axis. This option is not available when viewing a single trend. |