Notification Recipient Screen - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

See Setting up Device Notification.

Table 1. Notification Recipient Screen

Field

Description

ID

Indicates the ID of the device you want to send a notification to. ID field when selected.

IP Address

Indicates the IP address for the device you want to send notification to. Following fields when selected:

  • Address: The device IP Address.
  • Network Number: The network number of the device.
  • UDP Port: The UDP port number of the device.

Broadcast

Indicates if you want to broadcast the notification. Displays the following fields when selected:

  • Broadcast Type: The broadcast type: Local, Remote, or Global.
  • Network Number: For a remote broadcast, enter the network number.
  • UDP Port: The UDP port number of the device.

MSTP Address

Indicates if you want to send a notification to another controller. Following fields when selected:

  • Address: The MS/TP address of the controller.
  • Network Number: The network number of the device.

Process ID

Indicates the process ID of the device that receives the event notification messages.

Day Selection

Indicates the days you want the system to send notifications.

Time Selection

Indicates the time frame you want the system to send notifications.

Notify on these Transitions

Indicates the type of events to send notification: Off Normal, Fault, and Normal.

Notification Messages Should Be

Indicates if notifications need to be confirmed by a user.