Calendar View - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

See Adding a Basic Calendar or Referencing a Global Calendar.

Table 1. Calendar View

Button

Description

Local

Selects the local calendar option.

Global

Selects the global calendar option and opens the calendar location entry:

  • Device: The BACnet global identifier of the device.
  • Calendar: The BACnet global identifier of the calendar.

Go to the previous year.

Go to the next year.

Go to the previous month.

Go to the next month.

Go to today.

Use to view calendar details and define date ranges (for example, summer hours for an entire month). For more information about how to set up a date range, see Adding a Calendar with a Date Range.

Save

Saves changes to the information in the screen.

Cancel

Exits the screen without saving changes.

Opens the help system.