Calendar Details Screen - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

See Adding a Basic Calendar or Adding a Calendar with a Date Range.

Table 1. Calendar Screen

Field

Description

Object - Name

Indicates the name of the calendar.

Description

Indicates the description of the calendar.

Enabled

Indicates whether the calendar is enabled (True) or disabled (False).

Object Identifier

Indicates the read-only ID for the calendar.

BACnet - Present Value

Indicates if the current date is in the date list.

If the current date is in the date list, the Present Value will show a status of True. If the current date is not in the date list, the Present Value will show a status of False.

BACnet - Date List

Shows the dates in the calendar.

Global Calendar Update

Indicates that the calendar is being used from another device. This field appears in Commissioning mode only.