Commissioning a Device - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

Procedure

  1. Click the Commission button. The Commission Device Wizard appears.
  2. Choose the application transfer type and the connection type information.
    Note: To commission a device that contains an existing application, use the Applications in Controller setting to make sure you commission the latest information.
  3. Enter your connection parameters and click Next
  4. From the Device Selection screen, select a device.
  5. Click Next.
    Note: If the application type is Application in Controller and no devices appear on the Device Selection screen, click Discover.
  6. Click Finish. The application appears to be commissioned in the Control View.
    Notes:
    • If the application type is Application in Controller, the tool transfers the application from the selected device to the computer.
    • The Notice dialog box appears when the application version in the controller is older than the application version loaded in the Tool. You can continue commissioning this application successfully; however, you do not see any new items added since the last device update. Perform a transfer to the device to see new items.