Chiller Options (SP) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The selection options for Chiller Options are:

  • Chilled Water Options

    • Flow Switch: This option monitors the status of the chilled water flow through each chiller.

    • Flow Sensor: This option measures the chilled water flow through each chiller.

    • Entering Water Temp: This option monitors the entering (return) water temperature of each chiller.

    • Leaving Water Temp: This option monitors the leaving (supply) water temperature of each chiller.

  • Condenser Water Options

    • Flow Switch: This option monitors the status of condenser water flow through each chiller.

    • Flow Sensor: This option measures the condenser water flow through each chiller.

    • Entering Water Temp: This option monitors the entering or return water temperature of each chiller.

    • Leaving Water Temp: This option monitors the leaving or supply water temperature of each chiller.

  • Chiller Alarm: This option monitors the general alarm status of the chiller.

  • Chiller Setpoint Adjustment: This option generates an AO to the chiller to command the setpoint through the BAS.

  • Chiller Current Limit Adjustment: This option generates an AO to the chiller to command the current limit through the BAS.

  • Chiller Amperage: This option monitors the current of each chiller.

  • Primary Supply Temperature: This option monitors the primary supply water temperature.

  • Primary Return Temperature: This option monitors the primary return water temperature.

  • Primary CHW Flow Sensor: This option monitors the primary flow sensor.

  • Refrigerant Monitor Panel Alarm: This option monitors the refrigerant alarm.