Basin Options (SP) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
The selection options for Basin Options are:

  • Basin Level Alarm: This option monitors basin low level alarms.

  • Basin Heater Enable: This option generates BOs to command the basin heaters through the BAS.

  • Basin Water Temperature: This option monitors basin water temperatures.

    • Switch: This option monitors BI inputs for low temperature switches.

    • Analog Temperature: This option monitors AI inputs for temperature.

  • Basin Level Switch: This option monitors the basin levels.

  • Basin Makeup Valve: This option generates BOs to command basin makeup valves through the BAS.

If the No CW Piping (Air Cooled) node is selected, Basin Options cannot be selected.