Cooling System Enable (CC) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The selection option for Cooling System Enable is:

  • OA Cooling Lockout: This input is the setpoint, below which, the system is locked out or disabled.

  • Emergency Shutdown: This option allows the system to automatically shut down upon activation of a binary input.

  • Low Pressure Shutdown: This option allows the system to automatically shut down should the system pressure drop below a specified pressure.