Secondary Chill Water Options (CC) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The selection options for Secondary Chill Water Options are:

  • Supply Temperature: This option monitors the secondary loop supply temperature.

  • Return Temperature: This option monitors the secondary loop return temperature.

  • Flow Meter: This option monitors the secondary loop flow rate.

  • Decouple Temperature: This option monitors the decouple loop temperature.

  • Decouple Flow Meter: This option monitors the decouple loop flow rate.

  • Decouple Flow Direction: This option monitors the decouple loop flow direction.

  • Building Load Meter: This option monitors the secondary loop BTUs.