Primary Cond Water Pumps (CPO) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The condenser water systems consist of water cooled chillers, constant or variable speed condenser water pumps, and two-position or proportional isolation valves if the pumps are piped in parallel (common header).