Blocking Protection (CPO) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The Blocking Protection option provides monitoring of the command to a motor (typically a pump). If the command is off for an extended period of time (for example, 7 days), the motor starts for a short time (for example, 30 seconds). This feature prevents blocking (that is, it prevents the motor from seizing up).