No CW Piping (Air Cooled) (CPO) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The Air-Cooled Condenser system does not use condenser water to cool the chillers, since they reject their heat by having ambient air passed across refrigerant-to-air heat exchangers. In packaged air-cooled chillers, the manufacturers attempt to provide optimal performance by staging fans in response to chiller load and ambient, dry-bulb temperature.