General Options (CPO) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The selection options for General Options are:

  • Outside Air Temperature: This option monitors the outdoor air temperature.

  • Outside Air Humidity: This option monitors the outdoor air humidity.

  • Mechanical Room Temperature: This option monitors the temperature of the mechanical room.