Condenser Options (CPO) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The Common Return Temperature option monitors the condenser return water temperature. The Condenser Flow Sensor option monitors the condenser flow sensor.

If the No CW Piping (Air-Cooled) node is selected, Condenser Options cannot be selected.