Table 1 describes the Analog Value object commands. For information about command priorities, see Command Priority Levels.
|
Name |
Description |
|---|---|
|
Adjust |
Releases priorities 9–15 and sets Priority 16 to the value you enter in the command. Present Value (appears as O1) changes to the highest value in the priority table.
Note: This command is available only if the Analog Value is prioritized.
|
|
Operator Override |
Replaces Present Value (appears as O1) at the Operator Override priority with the value you enter in the command. The override has no effect if a higher priority value is in the Present Value attribute.
Note: This command is available only if the Analog Value is prioritized.
|
|
Release Operator Override |
Releases an Operator Override command.
Note: This command is available only if the Analog Value is prioritized.
|
|
Release |
Releases a specific priority of Present Value (appears as O1).
Note: This command is available only if the Analog Value is prioritized.
|
|
Release All |
Releases Priorities 3–15.
Note: This command is available only if the Analog Value is prioritized.
|
| Enable Alarms | Enables all types of alarming.
Note: This command is available only if the Analog Value is prioritized.
|
| Disable Alarms | Disables all types of alarming.
Note: This command is available only if the Analog Value is prioritized.
|