Supply Fans (SZAHU) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The discharge air setpoints and fan speed modulate to control the zone temperature to its setpoints. For more details, see ASHRAE Guideline36-2021 Single-Zone VAV Air-Handling Unit - Supply Fan Speed Control and Supply Air Temperature Set-Point Reset (Section 5.18.4).