Dehumidification Control (RTU) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

These selections provide the logic for dehumidification control.

The selection options for Dehumidification Control are:

  • Zone Humidity

  • Return Air Humidity

  • Activate Hot Gas Reheat during Dehumidification

Dehumidification cannot be selected unless both Cooling and Reheat are selected.