Configuration Options (MADD-MZ) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

These selections allow the user to select the portion(s) of the Multizone logic to include in this system. The selection options are:

  • AHU Only

    • Zone Heating Valve Mode Output

    • Zone Staged Heating Mode Output

  • Zones Only

  • AHU + Zones