Occupancy Control (MADD-MZ) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

These selections provide the logic for Occupancy Mode Determination.

The selection options for Occupancy Control are:

  • Always Occupied

  • Scheduled Occupancy

    • Override Support

    • Occupancy Switch (BI)

    • Unoccupied Strategy

      • Intermittent Night Operation

      • Off during Unoccupied

If any options are selected for separate Occupied and Unoccupied Setpoints or Temporary Occupancy, the Always Occupied option cannot be selected.