Zone Temperature (MASD) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

Selecting this option adds an analog input for the zone temperature and uses this value in the primary temperature control loop. Additional options allow the user to select a Setpoint Adjust feature, which can be of either Common Setpoint Adjust or Warm Cool Adjust type, or a Temp Occ Support option to support a request for temporary occupancy from the zone sensor.