Heat Recovery (MASD) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

This section defines an optional heat recovery device that exchanges heat between the exhaust air stream and the fresh air stream. These devices can be used for heating and cooling depending on the season.