Fans (MASD) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

All unit configurations must include at least one constant speed or variable speed supply fan. If you select a variable speed fan, a static pressure sensor is included to control the fan. You can also select Two Duct Static Pressure Sensors to add an additional sensor and low select between the two to control the fan speed. Two and three speed fans are not supported for Air Handling Units.