Economizer Damper(s) (MASD) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

These selections provide the logic for the Economizer Dampers. If no economizer control (Free Cooling) is required, these options should not be selected (use Two Position Min OA Damper instead).