Chilled Water (MASD) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The section is used to define the properties of a chilled water coil. This type of coil supports proportional, incremental, or two position control types, as well as several options.