Mixed Air Dual Duct Applications - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

See the following sections for information on this application’s logic and selections.

See the Upgrading System Files section for a list and description of the module and System Selection changes that were made since the last release of the tool.