Upgrading Radio Firmware - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

Procedure

  1. From the Tools menu, select Trunk Utilities > Upgrade Radio Firmware. The Trunk Utilities - Upgrade Radio Firmware wizard appears with the Connection screen active.
  2. Select the connection type and parameters and click Next. The Transfer to Device screen appears.
    Note: We strongly advise against using an NxE Passthru connection to transfer to multiple controllers due to potential communication loss during the process.
  3. Click Discover to begin the discovery process and locate devices. When devices are located, they appear in the main section of the Transfer to Device screen.
    Note: To end the Discover process, click Stop.
  4. Select the desired devices from the list.
    Note: If more than one device has the same Instance Number, the numbers display red in the device list.
  5. Select or clear the Force Radio Transfer check box depending on whether you want to force a radio code transfer to device.
  6. Select or clear check boxes next to the devices you want to transfer to.
  7. If you imported a device from a transfer template, select the device and click Get Device Info. The Get Device Info button only works for devices that were imported from a transfer template. This is because the transfer template does not store the device model or boot, main, and radio code versions.
  8. Click Finish. The radio code transfers to the devices.
  9. Check the progress of the operation as follows:
    • View the text in the Status column.
    • Click View Status. The Status dialog box appears showing current status of the operation. Click Refresh periodically to update the status. Click Copy To Clipboard to copy and paste the text to another word-processing program, such as Microsoft Notepad.
    • Click View Log. The Log dialog box appears showing the detailed operation log file. Click Refresh periodically to update the log. Click Copy To Clipboard to copy and paste the text to another word-processing program, such as Microsoft Notepad.
    • Click Clear Log if needed. This action clears the contents of the log file.
  10. When the transfer to device completes, click Done.