| Field | Description |
|---|---|
|
Connection Screen |
|
|
Connection Type |
Use to specify the connection type to use:
|
|
Connection Parameters |
NxE Passthru: Use to specify the following:
Note: The Ethernet fields allows you to connect directly to a site by entering in the site's user name and password.
Bluetooth: Use to specify the COM port and baud rate to use. MAP 4.2+ / BACnet Router: Use to specify the following:
When you first open the wizard, the default connection parameters for connecting to a MAP Gateway at version 4.2 are automatically displayed. If the connection parameters are modified, the values are stored in the wizard for future use. To restore the connection parameters to the default values, click the MAP 4.2 Default button.
Note: For further information about the MAP and common troubleshooting issues, refer to the Mobile Access Portal Gateway User's Guide (LIT-12011999).
ZigBee: Use to specify the Personal Area Network (PAN) Offset. |
|
Transfer Screen |
|
|
Browse Button |
Use to select the directory and file name of the transfer template file. |
|
Save Button |
Prompts you to browse for a directory and type a file name to save the transfer template file. |
|
Force Radio Transfer Check Box |
Use to force a radio code transfer to device. If this check box is not selected, the radio code is transferred to the device only if the code is different. If the check box is selected, the radio code is always transferred to the device. |
|
Devices Table |
Available devices, including:
|
|
View Status Button |
Opens the Status dialog box showing the current status of the operation. Click Refresh periodically to update the status. Click Copy To Clipboard to copy and paste the text to another word-processing program, such as Microsoft Notepad. |
|
View Log Button |
Opens the Log dialog box showing the detailed operation log file. Click Refresh periodically to update the log. Click Copy To Clipboard to copy and paste the text to another word-processing program, such as Microsoft Notepad. |
|
Clear Log Button |
Clears all contents of the log file. |
|
Get Device Info Button |
Use for devices imported from a transfer template (the transfer template does not store the device model or the boot, main, and radio code versions). The Get Device Info button retrieves the boot, main, and radio code values from the actual device so a transfer to device can be properly done. |
|
Discovery Button |
Starts the Discovery process for locating devices. |
|
Stop Button |
Stops the Discovery process. |
|
Navigation Buttons |
|
|
Previous |
Moves to the previous screen of the wizard. |
|
Next |
Moves to the next screen of the wizard. |
|
Finish/Done |
Finish starts the transfer. Done appears after the transfer completes. Click Done to close the wizard. |
|
Cancel |
Closes the wizard without performing the transfer. |
|
|
Opens the Help system. |