|
Field |
Description |
|---|---|
|
Connection Screen |
|
|
Connection Type |
Use to specify the connection type to use:
|
|
Connection Parameters |
NxE Passthru: Use to specify the following:
Note: The NxE Passthru fields allows you to connect directly to a site by entering in the site's user name and password.
Bluetooth: Use to specify the COM port and baud rate to use. Product Type radio buttons allows you to choose a communication parameter between Metasys or Facility Explorer based controller products. MAP 4.2+ / BACnet Router: Use to specify the following:
When you first open the wizard, the default connection parameters for connecting to a MAP Gateway at version 4.2 are automatically displayed. If the connection parameters are modified, the values are stored in the wizard for future use. To restore the connection parameters to the default values, click the MAP 4.2 Default button.
Note: For further information about the MAP and common troubleshooting issues, refer to the Mobile Access Portal Gateway User's Guide (LIT-12011999).
ZigBee: Use to specify the Personal Area Network (PAN) Offset. Product Type radio buttons allows you to choose a communication parameter between Metasys or Facility Explorer based controller products. |
|
Attribute Template Screen |
|
|
Browse Button |
Use to select the directory and file name of the attribute template file. |
|
Save Button |
Prompts you to browse for a directory and type a file name to save the attribute template file. |
|
Devices Table |
Available devices, including:
|
|
Read Attributes Button |
Reads current values from the selected devices. |
|
Write Attributes Button |
Writes updated attributes back to the devices. |
|
Copy to Clipboard Button |
Copies and pastes the text to another word-processing program, such as Microsoft Notepad. |
|
Discovery Button |
Starts the Discovery process for locating devices. |
|
Stop Button |
Stops the Discovery process. |
|
Navigation Buttons |
|
|
Previous |
Moves to the previous screen. |
|
Next |
Moves to the next screen. |
|
Finish |
Closes the wizard. |
|
Cancel |
Closes the wizard without saving. |
|
|
Opens the Help system. |