Box Fan (VAV-SD Slave) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The three selections for Box Fans provide the necessary State Generator, Output Controller, and Outputs based on the type of fan selected.

If an Exhaust Damper is selected, Box Fans cannot be selected.

The selection options for Box Fans are:

  • Parallel Fan Single Speed

  • Series Fan Single Speed

  • Series Fan Variable Speed

    • Series Fan Enable

  • Fan Status: This option creates a monitoring only point to use during commissioning or to map to the Supervisory system.