Sensors (VAV-DD Slave) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The selection option for Sensors/Inputs is:

  • Discharge Air Temperature: This option is used primarily as a monitoring feature during commissioning.