VAV Single Duct Mechanical System Selection - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04
Note:

During the System Selection Process, the application automatically creates a Discharge Air Velocity Pressure Input (DA-VP). For some VAV Controllers the signal type applied to the Analog Input is Integrated Digital Velocity Pressure. For other models, the signal type is Integrated Velocity Pressure. Depending on whether the controller being used requires digital or not, you will need to adjust the point's signal type accordingly.

For applications selections that do not use the built-in Velocity Pressure transducers found on the VAV Controller hardware (for example, Exhaust VAV Boxes or Dual Duct configurations), the signal type used for a separate analog input is typically the 0–10 VDC input type.