Temperature (VAV-SD) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

All applications require a zone temperature sensor. This input defaults to a SAB signal to use a net stat and not consume additional IO points. The Setpoint Adjust option allows you to choose either Common Setpoint Adjust or a Warm Cool Adjust. You may also optionally select to add Temp Occ Support to include an input for temporary occupancy requests.