Lighting (VAV-SD) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The Lighting option creates an output to interface a Lighting Relay. If the lighting option is selected, the Always Occupied selection in the Occupancy (VAV-SD) section is not available. Only the Occupancy Mode Determination Mode logic interfaces with the Lighting Output. The default output configuration is a single, maintained binary output.