Box Heating (VAV-SD) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04
Choose this option if your application includes a reheat coil downstream from the VAV box. Reheat coils may be one of three possible types:
  • Electric Staged coils can have up to three stages.
  • Hot Water (or steam) coils can use one of three possible signals.
    • Proportional Output creates an analog output to control the reheat valve.
    • Incremental Output creates two binary outputs to control a floating reheat valve.
    • Two Position Valve creates a single binary output to turn the reheat coil on and off.
  • Packaged Coil (SCR) adds an analog output to your application and controls it for an analog electric heating coil (SCR stands for Silicon Controlled Rectifier). The Include Heating Enable BO option adds a BO to enable as heating coil when needed.