Occupancy (VAV-DD) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The selection options for Occupancy are:

  • Always Occupied: This option sets the default value of Occupied for the ZN-T Setpoint Determination and Balancer Override modules to Occupied.

  • Scheduled Occupancy: This option creates the interface for the Supervisory system scheduling logic.

    • Override Support: This option creates the local override interfaces from optional Occupancy Sensors or Networked Sensor Temporary Occupancy interfaces.