Table 1 summarizes all of the possible Network Inputs created in the VAV Slave Dual Duct Applications and their corresponding Peer References to read from the Master VAV application.
Slave Application Network Inputs |
Master Application Object ID Type and Name |
Master Object ID Peer Reference |
---|---|---|
AUTOCAL-C |
Autocal State value from the Autocalibration Sequence (Autocalibration Sequence v50) State Generation module |
MV 3091 |
CD-OA% |
Network Input CD-OA% |
AV 10 |
EMERGENCY-MODE |
Smoke Sequence-State value from the Smoke Control Sequencing for UL-864-UUKL State Generation module |
MV 3915 |
HD-OA% |
Network Input HD-OA% |
AV 36 |
MSTRCDFLOW-OUTSTATE |
CDD-OUTSTATE parameter from the CD Damper Control module |
MV 3123 (Constant Flow) MV 3126 (Variable Flow) |
MSTRCDFLOW-PERCENT |
Damper % Command value from the CD Damper Control module |
AV 78370 (Variable Flow) AV 78241 (Constant Flow) |
MSTRHDFLOW-OUTSTATE |
HDD-OUTSTATE parameter from the HD Damper Control module |
MV 3224 (Constant Flow) MV 3226 (Variable Flow) |
MSTRHDFLOW-PERCENT |
Damper % Command value from the HD Damper Control module |
AV 78628 (Variable Flow) AV 78499 (Constant Flow) |
MSTRSUPHTG1-C Electric On Off |
Output SUPHTG1-C |
BO 2126 |
MSTRSUPHTG1-C Steam/Hot Water On Off |
Output SUPHTG1-C |
BO 2128 |
MSTRSUPHTG-O Incremental |
Output SUPHTG-O |
AO 2129 |
MSTRSUPHTG-O Proportional |
Output SUPHTG-O |
AO 2127 |
MSTRZN-CO2 |
Input ZN-Q |
AI 1100 |