Using the Help System - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

You can access both the online Controller Tool Help and the PDF to quickly find information. The tool supports context-sensitive help, which provides you with instant access to a help topic from a component in the user interface. However, in some instances, such as when searching with multiple keywords, the PDF provides the better option for finding information. To open a PDF of the help file, select Topics PDF in the Help menu.