Context-Sensitive Help - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
Context-sensitive help functions in multiple ways within the tool. Select a component of the user interface, such as a module, logic block, or dialog box, and press F1 to display the help topic for that selected component. For example, if you select the State Generation Tower Start Determination module and press F1, the Tower Start Determination help topic appears in your default browser. When viewing a dialog box, you can also click the help icon to display the help in your default browser.

When working within the System Selection Wizard, press F1 or click the Help icon () to display application information in the right pane. The upper-right pane includes application help content. The lower-right pane shows the relationship between the node selected in the left pane and other nodes within the tree. See the following figure.

Figure 1. Return Water Temperature Differential Example

The Selections Affecting table lists nodes that affect the node you currently have selected and the current status of these nodes. For example, if you select the Return Water Temp Differential node in the Type of Chiller Sequencing section of the tree, the Selections Affecting Return Water Temp Differential lists Variable Speed Pump with a status of Allow. This means that if Variable Speed Pump is selected, then Return Water Temp Differential is no longer selectable. When you select Variable Speed Pump while Return Water Temp Differential is selected, the Type of Chiller Sequencing option changes to Chiller Load because the Return Water Temp Differential option is no longer valid.

The Selections Affected by table lists nodes that may be unavailable or available based upon the current node selection. For example, if you select the Return Water Temp Differential node, the Selections Affected by Return Water Temp Differential section lists Primary Return Temperature and Primary Supply Temperature with a status of Disallow. This Disallow status means that if you select the Return Water Temp Differential node, the control logic selections under Chiller Options for Primary Return Temperature and Primary Supply Temperature become unavailable.

In the lowest section of the right pane, the Modules that may be laid down table lists modules that may be created based upon the current node selections. Some module names appear as links, which, when clicked, open a separate help window to a topic that provides information on that module or module category. For example, if you select the Chiller Load node, the Load Filter Module appears in the table. When you click Load Filter Module, the help topic for Load Filter appears in a separate window.

Figure 2. Load Filter Module Example

When working with the Global Sequencer Wizard, press F1 or click the Help icon () to display information for each page of the Global Sequencer Configuration Wizard.