Control Tab Screen - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The Control tab is part of the Classic View workspace. See Control Tab in the Classic View Workspace. See the Modes section for information on the modes of operation.

Table 1. Control Tab

Screen Area

Description

Module Sections

Modules used in the selected system in categorized sections. The flow of the content is from left to right where the inputs appear on the left, control/logic/state components are in the center, and outputs appear on the right. The module categories in the Control View are: