The Application tab is part of the Simple View workspace. See the figure in the Simple View section. See Simple View Workspace for information UI and its components.
|
Screen Area |
Description |
|---|---|
| Inputs Table | Lists the Inputs defined for the system. See Inputs. |
|
Parameters Table |
Lists the parameters/attributes of all modules that are exposed for connection () and to BACnet systems. Parameters are listed in alphabetical order. The components of the Parameters table are:
Note: You cannot modify outputs of modules from the Parameters table.
|
| Outputs Table | Lists the Outputs defined for the system. See Outputs. |