The Simple View perspective is built into the tool and always available.
The following figure shows the Simple View perspective of the user interface. The table describes the components.
|
Callout |
Screen Area | Description |
|---|---|---|
| 1 |
Menu Bar |
Includes the menus available in the tool. See the Menu Bar section. |
| 2 |
Mode Button Toolbar |
Use to switch between the modes of operation while working in the tool. The mode buttons are: See the Modes section for information on the modes and buttons. If desired, you can undock the Mode button toolbar and move it to a different area of the screen. |
| 3 |
Operation Buttons |
Use to perform specific tasks in the tool. The operation tasks and buttons are: See the Select System, Sideloop, and Define Hardware sections for descriptions of the operations. |
| 4 |
Navigation Tabs |
Application and System Selection Information tabs. See the Application Tab and System Selection Information Tab sections. |
| 5 |
Edit Button |
Use to edit parameters. |
| 6 |
Help Button |
Opens the Help system. |
| 7 |
Outputs Table |
Use to view and edit outputs. |
| 8 |
Inputs Table |
Use to view and edit inputs. |
| 9 |
Parameters Table |
List of modules and parameters. |
| 10 |
Status Bar - System |
Indicates the hardware assignment indicator, system capacity indicator, and system information link. See the Status Bar section. |
| 11 |
Status Bar - Application |
Indicates the current connection type, connection status, current mode, perspective name, and current release mode. See the Status Bar section. |
| 12 | Name | CAF Name or System Name in a clickable link format. If you click the name link, the System Information dialog box appears |