Perspectives - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
A perspective is a representation of the entire UI related to displaying data of an application, which includes all components except for menu, button, and status bars. You can build customized perspectives using a variety of containers and widgets.

Perspectives allow a simple view of an application without the complexity of the application shown by default. Perspectives also allow for customization of the UI to enable the user to more easily commission or understand an application.

See Perspectives.