Classic View - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The Classic View perspective is built into the tool and always available. When you first open an application, the tool defaults to the last used perspective of the application's system configuration. The following figure shows the Classic View perspective of the user interface. The table describes the components.

When you run a simulation or view live data in the commissioning mode, changing values are highlighted by a color. Colored highlighting is determined by the frequency that the value changes. As poll cycles return consistent values, the highlight fades away. This feature brings attention to changes throughout the application data system to expose potential relationships between values and modules and assist in troubleshooting.
Note: Temporary color highlights appear in three color stages (blue, yellow, and red). After the third stage (red) has been reached, all subsequent consecutive changes continue to display red. For more information on status color, see Table 1.
Figure 1. Classic View Perspective User Interface Screen

Table 1. Classic View Perspective User Interface Screen Details

Callout

Screen Area

Description

1

Menu Bar

Includes the menus available in the tool. See the Menu Bar section.

2

Mode Button Toolbar

Use to switch between the modes of operation while working in the tool. The mode buttons are:

See the Modes section for information on the modes and buttons.

If desired, you can undock the Mode button toolbar and move it to a different area of the screen.

3

Operation Buttons

Use to perform specific tasks in the tool. The operation tasks and buttons are:

See the Select System, Sideloop, and Define Hardware sections for descriptions of the operations.

4

Application Panel

Control and Logic tabs.

To make the Application panel a full screen, double-click the Application panel title bar.

5

Control and Logic Tabs

Use to navigate between the Control tab (system overview) and Logic tab. See the Control Tab and Logic Tab.

6

Minimize and Maximize Buttons

Use to minimize or maximize the Applications panel or the Features panel.

Note: You can also minimize or maximize the Applications panel or the Features panel by double-clicking the title bar.
7

Help Button

Opens the Help system.

8

Status Bar - Application

Indicates the current connection type, connection status, current mode, perspective name, and current release mode. See the Status Bar section.

9

Status Bar - System

Indicates the system name, hardware assignment indicator, system capacity indicator, and system information link. See the Status Bar section.

10

Features Panel

Use to view and work with key data. The Features Panel contains the following tabs:

To make the Features panel a full screen, double-click the Features panel title bar.

11

Slider Bars

The slider bars in all views are active and have arrows allowing you to expand the panels to achieve the desired view. Click the arrows to show and hide the panels. If you click the slider bar and drag it to the desired location, clicking the arrows returns the view to the location you moved the slider bar. Clicking the arrows a second time shows/hides the entire panel. Many, but not all, sliders maintain their location between sessions.

12

Classic View Workspace (Control Tab Shown in Figure 1)

Control tab or Logic tab contents settings. See the following sections for more information and details:

13 Name CAF Name or System Name in a clickable link format. If you click the name link, the System Information dialog box appears.