System - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

In the tool, a system is represented by the mechanical equipment and the logic needed to control that equipment, independent of hardware definition. The System Selection Wizard describes the make-up of a mechanical system to aid you in creating the group of logic components that work together to control the mechanical system. See System Types and Configurations in the Configuring a System section.