Settings - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The Settings menu includes the following options:

Table 1. Settings Menu Options

Option

Description

Perspective > Classic View

UI in the Classic View. This menu option is only available when an application is open.

Perspective > Simple View

UI in the Simple View. This menu option is only available when an application is open.

Perspective Management

Opens the Perspective Management dialog box, which enables you to create and edit perspectives.

Release Modes

Switches the application to use a different Release Mode for opening and creating new CAFs. For more information, see the Release Modes section.

Localization Opens the Localization screen.
Naming and Signal Opens the Naming and Signal screen.
System Selection Opens the System Selection screen.
Adjust Refresh Rate Opens the Adjust Refresh Rate dialog box, which allows you to change the refresh rate of Commissioning or Simulation sessions.
Hide Last Value Modules

Hides the Last Value modules when selected.

Hide Warning Flags Hides block warning flags.
Use Involvement Dialog Involvement summary in a dialog box.
Simulation Break Conditions

Opens the Break Conditions dialog box. This menu option is available in simulation and configuration mode.