Commissioning - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

Commissioning mode allows you to connect to a device and view actual data from that device. You can use this mode to monitor your device and set Offsets, COVs, and Polarity in addition to other Parameter and Detail changes. For example, you can change the Min Out and Max Out values of an Output to fine tune the range of a 2 to 10 VDC proportional valve. In addition, the Commissioning mode has a balancing feature for VAV applications to easily autocalibrate VAV boxes and set flow constants in one location. See the Commissioning a System section.

Back to Modes