Menu Bar - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The menu bar includes the following options:

Table 1. Menu Bar Options

Menu

Option

Keyboard Shortcut

Description

File

New

Ctrl + N

Opens the New System dialog box. See the Configuring a System section.

Open

Ctrl + O

Opens the Open dialog box to select an existing CAF to use.

The Controller Application File is found in the following default location:

C:\Users\<username>

Close

Ctrl + F4

Closes the open CAF. You must be in Configuration mode to close a CAF.

Disconnect from Archive  

Select this action to return CCT to normal operation while leaving the CAF open.

Note: This feature is only available when you launch CCT using the SCT.

Save

Ctrl + S

Saves the current system as a CAF. If you have not already saved the system, the tool opens the Save dialog box.

Invalid characters for CAF file names include:

: * ? " < > | / \

Save As

 

Opens the Save dialog box to allow you to save the system as a CAF using a different name.

Invalid characters include:

: * ? " < > | / \

Save a Copy

 

Use this feature to save a copy of the CAF without modifying the working copy.

Invalid characters include:

: * ? " < > | / \

Print

Ctrl + P

Opens the Summary Report Options dialog box to print a summary of the open CAF in PDF format.

Recent Files

Ctrl-0 through Ctrl-9

Opens a recently viewed CAF. This menu holds up to ten recent files.

Exit

 

Closes the software.

View

Reset Layout

F7

Restores any resized panels to default size.

Reset to Default Screen

F8

Restores view to one monitor.

Arrange Multiple Screens

F9

Arranges the view across multiple monitors.

 

Save Perspective Layout

F10

Saves any edits made to the perspective layout (custom perspectives only).

Restore Perspective Layout

F11

Discards any edits and restores perspective to the last saved version (custom perspectives only).

Tools

Box Flow Test

 

Opens the Box Flow Test feature. See the Box Flow Test Overview section.

Wireless > ZFR Channel Configuration

 

Opens the Wireless > ZFR Channel Configuration Screen.

Wireless > Upgrade ZFR Coordinators

 

Opens the Upgrade ZFR Coordinators wizard.

Wireless > Upgrade Single ZFR Coordinators   Opens the Upgrade Single ZFR Coordinator wizard.

Trunk Utilities > Transfer CAF and Attributes to Controller

 

Opens the Trunk Utilities > Transfer CAF and Attributes to Controller wizard. See the Working with the Trunk Utilities section.

Trunk Utilities > Transfer CAFs to Multiple Controllers

 

Opens the Trunk Utilities > Transfer CAFs to Multiple Controllers wizard. See the Working with the Trunk Utilities section.

Trunk Utilities > Upgrade Radio Firmware

 

Opens the Trunk Utilities > Upgrade Radio Firmware wizard. See the Working with the Trunk Utilities section.

Trunk Utilities > Read/Write Attributes Online

 

Opens the Trunk Utilities > Read/Write Attributes Online wizard. See the Working with the Trunk Utilities section.

Trunk Utilities > Manage Attribute Templates

 

Opens the Trunk Utilities > Manage Attribute Templates wizard. See the Working with the Trunk Utilities section.

Trunk Utilities > Transfer Controller CAFs to Computer

 

Opens the Trunk Utilities - Transfer Controller CAFs to Computer wizard. See the Working with the Trunk Utilities section.

Trunk Utilities > Upgrade Controller Software

 

Opens the Trunk Utilities > Upgrade Controller Software wizard. See the Working with the Trunk Utilities section.

Online Operations

 

When in Commissioning mode, opens the Online Operations dialog box to display information from the controller to which you are currently connected. See the Commissioning a System section.

When in Configuration mode, opens the Online Operations Wizard to send certain commands or display information from one or more controllers on a field bus. See the Configuring a System section.

Job Information

 

Opens the Job Information dialog box to enter information specific to the current job and the open CAF.

Upgrade System

 

Opens the System Upgrade dialog box to upgrade the open CAF to the latest version. See the Upgrading System Files section.

Bulk CAF Upgrade Utility

 

Opens the Bulk CAF Upgrade Utility screen. See the Upgrading System Files section.

CPO 10 Parameter Value Calculator

 

Opens the CPO 10 Parameter Value Calculator (PVC). The CPO 10 Parameter Value Calculator calculates the performance parameters of Central Plant Optimization 10 (CPO 10) systems for use in control modules of the tool.

Transfer Transfer To Computer (Upload) Ctrl + U Opens the Transfer Files wizard to transfer an application from the device to the computer.
Transfer to Device (Download) Ctrl + W Opens the Transfer Files wizard to transfer an application from the computer to the device.

Help

Topics

F1

Opens the online Help system.

Topics PDF

  Opens the Help PDF.

About Tool

 

Opens the About Tool dialog box displaying the tool version, Field Controller product version, tool library version, database version and patch information, and file version. See the About Tool Information section.